Define Operational Parameter
Operational parameters contain information about the current condition of the asset or system calculated using sensors. Example: operating pressure, velocity that changes with time. Perform the following steps to define the operational parameters.
-
Click Parameter > Operational tab.
-
Click Operational tab
When adding a record for any parameter under the Parameter section (Constructional, Operational, Derived, Predicted, or Physical Property), if a parameter is already associated with any of these categories, it does not appear in the add record parameter list. For example, if you add a record for a Constructional parameter, the same parameter is not available for selection in Constructional or any other listed categories.
-
Click Add Record button.
-
Select the operational parameters required for this template by selecting the check box next to them.
You can also search the required parameters using the search box in the top right corner of the window.
-
Click Add.